{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a document available for picking Telefast for Modicon X80 IO modules?
Issue
Want to use Telefast wiring solutions for the Modicon X80 IO and need help selecting modules.

Product line
Modicon X80 IO, Modicon M580, Modicon M340

Resolution
This information can be found in the IO module User guides. At the end of each modules individual chapter there is a Telefast wiring section.

The two documents are named:
Modicon X80 - Analog Input/Output Modules User Manual.
Modicon X80 - Discrete Input/Output Modules User Manual

They can be found on www.se.com

*** Note: There is no Telefast solution for the 16 channel Discrete IO modules. ***

Schneider Electric Canada