Search FAQs
Can the remote racking device for the MTZ be used on the NW breaker?
Issue:
Remote Racking device for MTZ and NW
Product Line:
Circuit Breakers
Resolution:
Yes, the Masterpact MTZ LV839292SP (whole kit) and LV839294SP (10 MTZ2-3 brackets only) can be used for the NW. The only difference is the size of the screws.
Remote Racking device for MTZ and NW
Product Line:
Circuit Breakers
Resolution:
Yes, the Masterpact MTZ LV839292SP (whole kit) and LV839294SP (10 MTZ2-3 brackets only) can be used for the NW. The only difference is the size of the screws.
Released for:Schneider Electric Canada
Explore more
Category:
Range:
Explore more
Category:
Range: