Search FAQs
Do you need the QOSAMK mounting kit to mount a SDSA1175 in a QO or Homeline Load Center?
Issue:
QOSAMK mounting kit application
Product Line:
Load Center
Environment:
Surge Protective Device
Cause:
Application
Resolution:
If the load center is installed in a flush mount application, the QOSAMK should be used. If the load center is installed in a surface mount application, the QOSAMK could be used or the surge arrester could be installed through a knockout in the load center enclosure.
QOSAMK mounting kit application
Product Line:
Load Center
Environment:
Surge Protective Device
Cause:
Application
Resolution:
If the load center is installed in a flush mount application, the QOSAMK should be used. If the load center is installed in a surface mount application, the QOSAMK could be used or the surge arrester could be installed through a knockout in the load center enclosure.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: