{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What Is the Replacement Overload Relay Control Circuit Contact For the Class 8536 Type S Starters with Melting Alloy Overload Relays?
Issue:
The melting alloy overload contact replacement

Product Line:
NEMA Contactors and Starters

Environment:
NEMA 8536 Type S Starters

Resolution:
Below are the part numbers.

Standard N.C. Contact Unit
Sizes 00 (SA)- 4 (SF) & 6 (SH) Series A & B = 9998SO1
Size 5 (SG) Series A = 31102-514-50
Size 5 (SG) Series B = 9998SO1

Standard N.C. Contact Unit Plus Isolated N.O. Alarm Contact
Sizes 00 (SA)- 4 (SF) & 6 (SH) Series A & B = 9999SO4
Size 5 (SG) Series A = Not Available
Size 5 (SG) Series B = 9999SO4

Standard N.C. Contact Unit Plus Isolated N.C. Alarm Contact
Sizes 00 (SA)- 4 (SF) & 6 (SH) Series A & B = 9999SO5
Size 5 (SG) Series A = Not Available
Size 5 (SG) Series B = 9999SO5

Schneider Electric Canada