{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the replacement overload relay for the 8536SB starters?

Issue:
Identify the replacement overload relay for 8536SB starters

Product Line:
NEMA Contactors and Starters

Environment:
Products sold in the US

Resolution:
Class 9065 Type SDO5 for melting alloy, or Class 9065 Type SDO6B (Form B) for ambient compensated bimetallic, or Class 9065 Type SDO6B2 (Form B2) for non-ambient compensated, or Class 9065 Type SS010 (Form H10 - now obsolete) for trip class 10 solid state overload, or Class 9065 Type SS020 (Form H20 now obsolete) for trip class 20 solid state overload, or Class 9065 Type SF020 (Form H30) for selectable trip class 10/20 solid state overload.

The class H10 and H20 are now obsolete and must be replaced with the 9065SF020.


Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: