Search FAQs
Are duplex motor controllers available for single-phase motors?
Issue:
Can the duplex motor controllers be factory wired for single phase?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Class 8941 Duplex AC Motor controllers
Resolution:
Yes, select the NEMA size required based on motor voltage & HP rating from the application data page of the digest. Once you have determined which NEMA size is required, turn to the 8941 section and select the duplex controller. Add form Y177 to have the factory wire it for single phase. This is a No Charge option however Horsepower and Motor Voltage must be supplied. No Exceptions! Order must be entered manually; this option is not available in the Quote to Cash Product Selectors.
Can the duplex motor controllers be factory wired for single phase?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Class 8941 Duplex AC Motor controllers
Resolution:
Yes, select the NEMA size required based on motor voltage & HP rating from the application data page of the digest. Once you have determined which NEMA size is required, turn to the 8941 section and select the duplex controller. Add form Y177 to have the factory wire it for single phase. This is a No Charge option however Horsepower and Motor Voltage must be supplied. No Exceptions! Order must be entered manually; this option is not available in the Quote to Cash Product Selectors.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: