Search FAQs
9007C54K Does it include the Wobble Stick Wire Extension?
Issue:
Is the wobble stick wire extension included on part number 9007C54K?
Product Line:
9007C Limit Switch
Environment:
NEMA Limit Switches
Resolution:
Yes, this is a complete 9007C limit switch, with 1 NO 1 NC contacts and the Wobble Stick Wire Extension.
Is the wobble stick wire extension included on part number 9007C54K?
Product Line:
9007C Limit Switch
Environment:
NEMA Limit Switches
Resolution:
Yes, this is a complete 9007C limit switch, with 1 NO 1 NC contacts and the Wobble Stick Wire Extension.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: