Search FAQs
How many keys come with a PK4FL, PK5FL, or PK22FL?
Issue:
Number of keys included in PK4FL, PK5FL or PK22FL locks
Product Line:
Load Center
Resolution:
One key (NSR251) is supplied as part of the hardware bag assembly with each trim. If a PK4FL, PK5FL, or PK22FL is ordered separately, no keys are supplied. The key must be ordered as LP9618 (1 key).
Number of keys included in PK4FL, PK5FL or PK22FL locks
Product Line:
Load Center
Resolution:
One key (NSR251) is supplied as part of the hardware bag assembly with each trim. If a PK4FL, PK5FL, or PK22FL is ordered separately, no keys are supplied. The key must be ordered as LP9618 (1 key).
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: