Issue:
9001SKT 120V Blue LED light module selection
Product Line:
Push Buttons and Operator Interface
Environment:
30 mm Illuminated Push buttons and selector switches
Resolution:
Yes. We have a new series of light modules available in 24 and 120 volts AC/DC. They use the same part numbers 9001 KM35L* and 9001 KM38L*, where * is replaced by the color code letter. Ex. 9001 KM35LL is 24 volt blue.
9001SKT 120V Blue LED light module selection
Product Line:
Push Buttons and Operator Interface
Environment:
30 mm Illuminated Push buttons and selector switches
Resolution:
Yes. We have a new series of light modules available in 24 and 120 volts AC/DC. They use the same part numbers 9001 KM35L* and 9001 KM38L*, where * is replaced by the color code letter. Ex. 9001 KM35LL is 24 volt blue.