Search FAQs
Are any of the PK ground bar kits, commonly used in QO and HOMELINE load centers, UL Listed?
Issue:
Are PK Ground Bar Kits, commonly used in QO and HOMELINE load centers, UL Listed?
Product Line:
PTFDS - FD Enclosure Systems
Resolution:
The following PK__GTA ground bar kits are UL Recognized Components - Panelboard Accesories, listed in File E6294, Volume 7, Section 31: PK3GTA1, PK4GTA, PK5GTA, PK7GTA, PK9GTA, PK9GTA1, PK12GTA, PK15GTA, PK15GTAFT, PK15GTAL, PK15GTA6, PK18GTA, PK18GTAL, PK23GTA, PK23GTAL, PK27GTA, PK32DTGA and PKGTAB.
The CCN (Component Category Number) is QEUY2.
Are PK Ground Bar Kits, commonly used in QO and HOMELINE load centers, UL Listed?
Product Line:
PTFDS - FD Enclosure Systems
Resolution:
The following PK__GTA ground bar kits are UL Recognized Components - Panelboard Accesories, listed in File E6294, Volume 7, Section 31: PK3GTA1, PK4GTA, PK5GTA, PK7GTA, PK9GTA, PK9GTA1, PK12GTA, PK15GTA, PK15GTAFT, PK15GTAL, PK15GTA6, PK18GTA, PK18GTAL, PK23GTA, PK23GTAL, PK27GTA, PK32DTGA and PKGTAB.
The CCN (Component Category Number) is QEUY2.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: