{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are the ZB2BE102 and ZBE102 interchangeable?

Issue:
Identify if the ZB2BE102 and ZBE102 blocks are interchangeable.

Product Line:
Push Buttons and Operator Interface

Environment:
22 mm Push Buttons

Resolution:
No. The ZB2BE102 is a contact block used with ZA2 and ZB2 operators, the ZBE102 is used on the ZB4 and ZB5 operators. The contacts mount to the collar differently and are not interchangeable.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: