{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which QO circuit breakers can be used on a 240 Vac corner ground delta (grounded B phase)?
Issue:
Are there specific QO/QOB breakers that can be used for a 240 V grounded B phase power source?

Product Line:
NQ Panelboards

Resolution:
A 2p breaker must be a QO-H or QOB-H type. These are labeled for corner grounded applications. See attached for more information.

Schneider Electric Canada

Attachment(s)
2700DB0202 2012.pdf [124.08 KB]