{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

To what air ambient temperature are the UL listed Multi9 miniature circuit breakers calibrated?

Issue:
To what air ambient temperature are the UL listed Multi9 miniature circuit breakers calibrated?

Product Line:
Miniature Circuit Breakers

Resolution:
UL listed Multi9 miniature circuit breakers C60BP/BPR/SP are calibrated at 25°C / 77°F air ambient reference temperature.
Derating table is available in the Multi9 catalog section LVCATM9OEM_EN for other air ambient operating temperatures from -30°C to +70°C / -22°F to 158°F.

Schneider Electric Canada