{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the replacement coil cover for 8502SA__ contactor or 8536SA___ starter?

Issue:
Is there a replacement coil cover for NEMA size 0 Contactor/Starter?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Contactors and Starters

Resolution:
31127-013-01 (Not available), secured by (2) 21937-14341 mounting screws. Cover does not include nameplate nor is nameplate available.

This also applies to all 8536SA, 8538SA, 8539SA, 8606SA, 8630SA, 8640SA, 8702SA, 8736SA, 8738SA, 8739SA, and 8810SA devices.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: