{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a breaker available for heat trace application?
Issue:
Is there a single pole 20A 120V heat trace breaker?

Product Line:
Miniature Circuit Breakers

Resolution:
Yes. Use the 1p QO-EPD breakers at 120 Vac or 1p EDB-EPD breakers for 277 Vac.

Schneider Electric Canada