{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: Installing HRK4060 Class R Fuse Kit on Heavy Duty Safety Switches

Issue:
How is a HRK4060 Class R Fuse Kit installed into the correct Heavy Duty Safety Switch fuse clips?

Product Line:
Heavy Duty Safety Switches

Environment:
Class R Fuse Rejection Kit

Resolution:
NOTE: The HRK4060 Class R fuse kits are design to be installed in the switches to REJECT all But Class R fuses. The Kit contains three rejection pins and collars, one per pole of a 3-pole switch.

The HRK4060 is designed ONLY for use with 400amp to 600amp, 240Vac and 600Vac Heavy Duty Safety Switches.

Also, follow ALL the steps in the instructions.(See below attached the kit instructions)
The equipment must be installed and serviced only by qualified electrical personnel.
Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.

Danger image

CAUTION: TURN OFF AND DISCONNECT POWER AHEAD OF SWITCH BEFORE INSTALLING FUSE ADAPTERS.
DO NOT USE RENEWABLE LINK FUSES IN FUSED SWITCHES.

Once all Safety steps are followed, begin the kit installation by following the steps in the instructions.
1) Insert the long pin through the hole in the load side fuse clip, and then through the collar.
2) Push the collar FIRMLY onto the pin. A pair of pliers may be required to push the collar onto the rejection pin. The collar should not be removable once properly installed.
NOTE: BE CAREFUL NOT TO BREAK ADJACENT MOLDED INSULATORS WHEN INSTALLING ADAPTER KIT.

Schneider Electric Canada

Attachment(s)

HRK4060 Instructions.pdfHRK4060 Instructions.pdf [142.1 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: