{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the step down Control Power Transformer voltage code for 600 to 120 VAC?
Issue:
Voltage Codes for 9070 Transformers

Product Line:
LV Transformers

Environment:
Applies to LV Transformers by SquareD/Schneider Electric

Cause:
9070 Industrial Control Transformers have various primary and secondary voltages


Resolution:

An Industrial Control Transformer with a 600V primary and a 120V secondary has a voltage code D5.  Example:  9070T100D5.


CTA-ID : 870

Schneider Electric Canada