{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is required to convert Class 8538 Type SBG11 Series D combination starter from non-fusible to 30-amp 250 volt fusible?
Issue:
How to convert a non fusible combination starter 8538 SBG11 Series D to 30-Amp 250V fusible?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 8538 Type SBG11 Series D Combination Starter

Resolution:
Class 9422 Type TC30 conversion kit is available to convert to 30-amp 250 volt fusible, but if modified the following consequences could occur.
(1) The local inspector checks and finds that the catalog number listed on the product nameplate does not match the modified product itself, the equipment could be red tagged.
(2) Should the equipment at some time need to be re-ordered and is simply re-ordered per the nameplate, upon receipt of new unit this conversion would be required again.

* Replacement product nameplates are not available.

Schneider Electric Canada