{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can 8903L/LX lighting Contactors be ordered with Normally Closed Power Poles?
Issue:
Needs to know how to order an 8903L lighting contactor with factory configured normally closed power poles

Product Line:
8903 Lighting Contactors

Environment:
NEMA Lighting Contactors

Resolution:
The first digit for 8 poles or fewer devices represent the normally open power poles and the second digit represents the normally closed power poles. For example, Class 8903 Type LO60 provides 6 normally open power poles where Type LO06 provides 6 normally closed power poles and Type LO33 provides 3 normally open and 3 normally closed power poles.

On 10 and 12 pole devices normally open is represented by the first two digits and normally closed by the last two digits .For example, Class 8903 Type LO1200 provides 12 normally open power poles where Type LO0012 provides 12 normally closed power poles and Type LO66 provides 6 normally open and 6 normally closed power poles. There is a maximum of 8 normally closed power poles when used in conjunction with normally open poles.

Schneider Electric Canada