{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the electrical interlocks available for ALL the current heavy duty safety switches?

Issue:
What electrical interlock kits are available for heavy duty safety switches?

Product Line:
Safety Switch

Resolution:
NOTE: FOR OLDER SERIES SWITCHES NOT SHOWN IN BELOW TABLES, SEE THE SWITCH WIRING DIAGRAM LOCATED ON THE BACK OF THE FRONT COVER

See the below tables for the electrical interlock kits for current series of heavy duty safety switches:
Interlock kit table
[59] For series not shown in table, refer to the switch wiring diagram
[60] Electrical interlock kit catalog numbers ending in 1 indicates one normally open and one normally closed contact. These kits use a 9007A01 industrial snap switch. Electrical interlock kit catalog numbers ending in 2 indicates two normally open and two normally closed contacts. These kits use a 9007C03 industrial snap switch.


For fiberglass reinforced polyester enclosures, NEMA Type 4X, 3 Pole, 600 Vac/dc, heavy duty safety switches, see table below:
Fiberglass reinforced polyester table
For krydon enclosures — NEMA Type 4X, 3 Pole, 600 Vac/dc heavy duty safety switch, see table below:
Krydon table

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: