{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for an SC1624M125F, Series M01?
Issue:
Product design repair parts

Product Line:
Combination Service Entrance Devices

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field replaceable:
Meter Cover - 40561613350
Meter Cover Mounting Screws - 4020513002K (contains 10 screws; only two screws are required to secure the meter cover)
Meter Sealing Ring - 2920910001
Utility Pullbox Cover - 4056172250 (includes latch)
Utility Pullbox Cover Sealing Screw - X1299
Load Center Cover - 4056131452 (includes hinges)
Load Center Cover Mounting Screws - (4) 2142217101
Dead Front Interior Trim - 4056188101
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only one screw is required to secure the interior trim)
Load Center Interior - 4056187050 (main breaker not included)
Load Center Interior Mounting Screws - (8) 2153217161
Main Breaker - HOM2125
Meter Base Assembly - 4056210750 (includes meter base with the right, load side meter jaw, blade guide, and straight connector assembled to the meter base)
Meter Jaw - (4) 7329794850
Meter Jaw Mounting Bolt - (4) 2271020242
Meter Jaw Mounting Keps Nut - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Line Side Phase Lugs - (2) 4025102451
Line Side Phase Lugs Mounting Bolt - (2) 2271020242
Line Side Phase Lugs Mounting Keps Nut - (2) 2342702001
Line Side Neutral Lug - LK100AN
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: