{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for an SC816F200F, series M01?
Issue:
Design Repair parts

Product Line:
Combination Service Entrance Devices

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4053442852
Meter Cover Mounting Screw - 4020513001K (contains 10 screws; only one screw is required to secure the cover)
Branch Wiring Gutter Cover (Below Meter Cover) - 4056178101
Branch Wiring Gutter Cover Mounting Screw - 404020513001K (contains 10 screws; only one screw is required to secure the cover)
Utility Pullbox Cover - 4056181150 (includes cover latch)
Utility Pullbox Cover Sealing Screw - X1299
Load Center Cover Assembly - 4056181250 (includes hinges)
Load Center Cover Mounting Screws - (2) 2142217101
Dead Front Interior Trim - 4056188501
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only two screws are required to secure the interior trim)
Load Center Interior - 4056188350 (main breaker not included)
Load Center Interior Mounting Screw - (2) 4020510001, (1) 4020511201, and (2) 4020516101 (3" long wire guide screws)
Main Breaker - QOM2200VH
Meter Base - 4054102503 (phenolic base; line and load phase jaws not included)
Meter Base Mounting Screw - 2142717200
Meter Jaw - (4) 7329794850
Meter Jaw Mounting Keps Nut - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Meter Sealing Ring - 2920910001
Left Line Side Phase Lug - 4025116051
Left Line Side Phase Lugs Mounting Bolt - 2271020242
Left Line Side Phase Lugs Mounting Keps Nut - 2342702001
Right Line Side Phase Lug and Line Side Neutral Lug are not field repairable.
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: