{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the torque requirement for the AL400LA lug for the LA, LH, and Q4 circuit breakers?

Issue:
Torque value for the AL400LA lug for the LA, LH, and Q4 circuit breakers.+

Resolution:
The torque requirement for the wire binding screw is 375 lb-in (42 N-M). The lug mounting screw torque value is 120 lb-in (13 N-M). Please see instruction bulletin 48040-896-03.

Schneider Electric Canada

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: