{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many keys are supplied with a PK4FL lock kit?
Issue:
How many keys are included with a PK4FL lock kit?

Product Line:
Load Centers

Resolution:
The PK4FL used to be supplied with one key. One key (NSR251) is currently supplied as part of the hardware bag assembly with each panel trim. If a PK4FL is ordered separately, no keys are supplied. The key must be ordered as LP9618. The LP9618 is 1 key. This change was effective March of 2004.

Schneider Electric Canada