{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the flame rating per UL 94 for the QOU?

Issue:
Do QOU breakers have a V0 flame rating as per UL94?

Product Line:
Miniature Circuit Breakers

Resolution:
All QOU frames use a UL recognized material (BMC 605) which has a flame class V-0.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: