{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the lengths of the leads on the SDSA1175T and SDSA1175 surge protective devices (SPDs)?

Issue:
Lead length inquiry for the SDSA11775 and SDSA1175T.

Product Line:
SPD

Environment:
SDSA1175

Resolution:
The surge protective device (SPD) leads consist of 600V 105°C 14 AWG wires, each approximately 2 feet in length.

Schneider Electric Canada

Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: