{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are replacement control coils available for 8965DPR63V02?
Issue:
8965DPR63V02 120 Vac coil replacement

Product Line:
Contactors and Starters

Environment:
Reversing Hoist Contactors

Resolution:
Requires (2) 9998DA2V02, coil consumption is 109 VA inrush and 10 VA sealed.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: