{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for an H225N, Series E2 or E4?
Issue:
Repair parts

Product Line:
HD Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Complete interior - HN225NE2 (includes line & load base assemblies, neutral assembly with bonding strap, arc suppressor assembly, box insulator, line & load phase insulators, and mounting hardware)
Line base assembly - 4055218850 (2 required; arc suppressor assembly not included)
Load base assembly - 4055219050SEL (2 required)
Arc suppressor assembly - 4051204501 (2 required)
Lug assembly - 4025113650 (1 required per base assembly)
Neutral assembly - 4055225250SEL
Neutral bonding assembly - 4028337950SEL
Line base phase insulator - 4051201401(1 required)
Load base phase insulator - 4055219101 (1 required)
Line and load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217251
Handle knob kit - Series E2 is 4401142750, Series E4 is 4028343550
Door thumb screw and retainer - 4405043401 & 4405049001
Cross Arm Insulator – (2) 4055217701 (left and right side pieces); (1) 4055217801 (center piece); (1) 4055215701 (dust shield – retainer for insulators)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: