{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for an H225NR Series E2, E4, and E5 heavy duty safety switch?
Issue:
Repair parts

Product Line:
HD Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Complete interior - HN225NE2 (includes line and load base assemblies, neutral assembly with bonding strap, arc suppressor assembly, box insulator, line and load phase insulators, and mounting hardware)
Line base assembly - 4055218850 (2 required; arc suppressor assembly not included)
Load base assembly - 4055219050SEL (2 required)
Line and load base mounting screws - 4020600901 (2 required per base assembly)
Arc suppressor assembly - 4051204501 (2 required)
Lug assembly - 4025113650 (1 required per base assembly)
Neutral assembly - 4055225250SEL
Neutral bonding assembly - 4028337950SEL
Handle assembly - 4051217251
Handle knob kit - series E2 is 4401142750, series E4 or E5 is 4028343550
Door thumb screw and retainer - 4405043401 and 4405043301 (series E5 only)
Cross Arm Insulator – (2) 4055217701 (left and right side pieces); (1) 4055217801 (center piece); (1) 4055215701 (dust shield – retainer for insulators)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: