{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is a general purpose EE or EXN Ventilated Transformer rated for damp locations such as a construction site, in buildings, but no side walls?
Issue:
Transformers in damp locations

Product Line:
LV Transformers

Environment:
Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Variety of installation environments

Resolution:
Low voltage general purpose EE or EXN Ventilated Transformers are in a Nema 2 `dripproof` enclosure; when energized the units will generate sufficient heat so as to not allow condensation.
The described location will also allow water at angles other than vertical (dripping), and thus the addition of an optional weathershield kit is necessary to achieve a Nema3R rating for outdoor applications.


Schneider Electric Canada