{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the conductor temperature rating for the main breaker lugs and the main lugs of QO or HOMELINE load centers?
Issue:
Product Design Features

Product Line:
QO and Homeline Load Centers

Resolution:
The lugs are suitable for 75°C conductors. 90°C conductors may be used if installed in accordance with the 75°C wire tables of the current NEC (National Electrical Code).

Schneider Electric Canada