{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for an H367, series E4 heavy duty safety switch?
Issue:
H367 Series E4 Heavy Duty Safety Switch Field Replaceable Parts.

Product Line:
Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4401119750 (3 required; arc suppressor assembly not included)
Load base assembly - 4401139350 (3 required)
Arc suppressor assembly - 4401139450 (3 required)
Lug assembly - 4405005302 (1 required per base assembly)
Line base phase barrier - 4401119501 (2 required)
Line base insulating plug - 4401133901
Handle assembly - 4401141351
Door thumb retainer - 4405049001
Door thumb screw - 4405043401
Handle knob kit - 4028343550
Crossbar Insulator Kit - 4051275250 (note: the metal cross bar is not replaceable)
Fuse Mounting Hardware - Bolt = 2140128481, Nut = 2342702800, Washer = 2360100280

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: