{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are replacement thermal unit mounting screws available for the 8536 Type S starters?
Issue:
What is the part number of the replacement thermal unit mounting screws for 8502/8536 Type S contactor/starters?

Product Line:
Class 8536 Starters

Environment:
Class 8502/8536 Contactors and Starters

Cause:
There is no description listed for the screw

Resolution:
Yes, the following outlines the required screw dependent upon device NEMA size. Each thermal unit will require two screws.

8536SA NEMA Size 00 through 8536SD NEMA Size 2 = 21920-16160

8536SE NEMA Size 3 & 8536SF NEMA Size 4 = 21943-22281

8536SG NEMA Size 5 Series A = 21401-24200 screw, 23701-00240 lock washer, and 23603-00244 washer.

8536SG NEMA Size 5 Series B = 21920-16160

8536SH NEMA Size 6 = 21920-16160

8536SJ NEMA Size 7 = Thermal units are not used, SSOLR.

Schneider Electric Canada