Search FAQs
Do the single phase, QO, convertible load centers have copper bus?
Issue:
Product design features
Product Line:
QO Single Phase Load Centers
Resolution:
Yes, ALL of the single phase, QO, convertible load center catalog numbers have tin plated copper bus.
NOTE: The main neutral bar and branch neutral bars are tin plated aluminum and NOT available in copper.
Product design features
Product Line:
QO Single Phase Load Centers
Resolution:
Yes, ALL of the single phase, QO, convertible load center catalog numbers have tin plated copper bus.
NOTE: The main neutral bar and branch neutral bars are tin plated aluminum and NOT available in copper.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: