{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Does the QO2175SB need to be hard-wired?

Issue:
QO2175SB Surge Protective Device Termination in QO™ Load Center

Product Line:
Surge Protective Devices (SPDs)

Environment:
Installation Method

Resolution:
The QO2175SB is a plug-on surge protector designed for QO load centers. It includes a white wire that must be connected to the panel's neutral bus. For optimal installation, place the QO2175SB as close as possible to the neutral assembly and main circuit breaker or main lugs.

Schneider Electric Canada

Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: