{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Will XALD or XALK enclosures accept XB4 operators?
Issue:
Can metallic operators be used in the plastic XALD and XALK control stations?

Product Line:
Push Buttons and Operator Interface

Environment:
22mm pushbuttons and control stations

Cause:
Product selection

Resolution:
No. You must use the ZB5 operators.

(Suggest XAP enclosures for XB4 operators.)

Schneider Electric Canada