{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can an 8536 non-reversing starter be converted to a reversing starter?
Issue:
Wants to convert an 8536 non-reversing starter to a reversing starter.

Product Line:
NEMA Contactors and Starters

Environment:
8536 Type S NEMA Starters

Resolution:
Yes. The following additional components will be needed: an additional 8502 contactor of the same NEMA size, a mechanical interlock, and two auxiliary interlocks.

Schneider Electric Canada