Search FAQs
What is the difference between the 9007CO3A and the 9007CO3B, and can a 9007C03 be substituted?
Issue:
What does the letter indicate at the end of the 9007CO3* part number?
Product Line:
Pressure, Vacuum, and Float Switches
Environment:
9007C Limit Switches
Resolution:
The 9007CO3A is a 2-NC snap switch. The 9007CO3B is a 2-NO snap switch. The 9007C03 is 2-NO + 2-NC and can be substituded for the -A and -B.
What does the letter indicate at the end of the 9007CO3* part number?
Product Line:
Pressure, Vacuum, and Float Switches
Environment:
9007C Limit Switches
Resolution:
The 9007CO3A is a 2-NC snap switch. The 9007CO3B is a 2-NO snap switch. The 9007C03 is 2-NO + 2-NC and can be substituded for the -A and -B.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: