{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Do the UL 489 listed Multi 9 breakers have DC ratings?

Issue:
Are Multi 9 breakers available with DC ratings?

Product Line:
Multi 9 Breakers

Resolution:
The single pole, 120/240 V breakers (e.g. M9F42103) have a 60 Vdc rating and the two pole, 120/240 V Multi 9 breakers (e.g. M9F42203) have a 125 Vdc rating.

Schneider Electric Canada