{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How can a customer tell what the AC coil voltage is installed in a TeSys D - line contactor?

Issue:
Identify the coil voltage in a TeSys D - line contactor

Product Line:
TeSys D-line contactors

Environment:
IEC Contactors and Starters

Resolution:
On 80A and below D-line contactors:
At the back of the top of the contactor there's a "viewing window".
You can see both the voltage code and the voltage through this "window".
On 115A and 150A D-line contactors there is not a viewing window but the voltage is stamped on the white
Bakelite piece behind L3.

Schneider Electric Canada