{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What does a "triple rating" mean in terms of an industrial control transformers voltage code? Example: 9070T250D1

Issue:
Explain the term triple rating, in terms of an industrial control transformers voltage code.

Product Line:
Transformer

Environment:
class 9070 Industrial Control Transformer

Cause:
Triple rating on Industrial Control Transformers

Resolution:
A triple rating on the control transformer`s voltage code basically means that the transformer is designed to successfully operate at voltages slightly different than the nominal voltage at it`s full VA capacity. This is done to allow for different voltage systems that require the same voltage ratios, say 4:1 or 2:1. Units with triple ratings are clearly marked in the Digest 172 with the triple rating expressed on page 12-13.

Example: The 9070T250D1 is a triple rated voltage code unit that can supply 250VA with the following input voltages and the corresponding output:

Input: 240 or 480
Output: 120

Input: 230 or 460
Output: 115

Input: 220 or 440
Output: 110

Schneider Electric Canada