{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Would a soft start be a suitable device for a crane hoist application?

Issue:
Soft start suitable for crane hoist

Product Line:
Starters

Environments:
Starters

Causes:
Catalog Selection

Resolution:
Hoisting application on a crane is not a good application to use a soft start on because of the reduced starting torque. It may be possible to use on other parts of the crane as long as they do not require rated torque at start-up. If a lot of torque is needed and soft starting is required may want to go with a drive.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: