{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many auxiliary contacts can be installed on a NEMA size 0, 1, or 2 reversing contactor or starter?
Issue:
Identify the number of auxiliary contacts that can be installed in a NEMA contactor or starter

Product Line:
8536/8502 NEMA Contactors and Starters

Environment:
NEMA Contactors and Starters

Resolution:
Qty (4) are allowed for each 2- or 3-pole contactor; however, they must all be installed on the outer side of the contactor, as the mechanical interlock between the contactors prevents any auxiliary contacts from being installed on the inner side. The auxiliary contacts are "stacked", or "mounted in tandem" on the outer side of each contactor. When adding 4 external auxiliary contacts to one Size o or 1 contactor, remove one of the return springs. Refer to 9999 SX auxiliary contact instruction bulletin.

Schneider Electric Canada