{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is 256 volt replacement control coil available for LC1D15000?
Issue:
LC1D15000 Replacement coil of 256V Part number

Product Line:
IEC Contactors and Starters

Environment:
Tesys D Contactors

Resolution:
256 volt control is not an option on theses contactors. Average coil consumption is 300 VA inrush 22 VA sealed for 50 hertz, 300 VA inrush 22 VA sealed for 60 hertz and 280 to 350 VA inrush 2 to 18 VA sealed for 50/60 hertz.

Schneider Electric Canada

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: