{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is a handle tie available for the two outer poles of two QOT tandem circuit breakers?
Issue:
Handle Tie for the Outer Pole on Two Adjacent Single Pole QO Tandem Circuit Breaker.

Product Line:
Circuit Breakers

Environment:
QO Tandem Circuit Breaker

Resolution:
No. Only the inside poles of two adjacent, single pole QO or QOT tandem circuit breakers can be handle tied (with QOTHT).

Schneider Electric Canada