{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where is the best place to mount a QO2175SB secondary surge arrestor in a QO load center?
Issue:
Product installation feature

Product Line:
QO load centers and Surge protective devices

Resolution:
The QO2175SB can be mounted anywhere in the QO panel, but ideally should be located as close to the mains as possible. The neutral conductor should be routed and connected to the panel's neutral assembly in the shortest distance possible.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: