{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can two branch neutral wires (or grounded conductors) be installed in the same neutral bar terminal in a QO or Homeline load center?

Issue:
Product Features

Product Line:
QO and HOMELINE Load Centers

Resolution:
No. The National Electrical Code (NEC) does NOT allow for this and the article in the current code would read something similar to this; "Each grounded conductor shall terminate within the panelboard in an individual terminal that is not also used for another conductor. Exception: Grounded conductors of circuits with parallel conductors shall be permitted to terminate in a single terminal if the terminal is identified for connection of more than one conductor."

Schneider Electric Canada