Search FAQs
Can you use molded case switches in place of a KAL/KHL breaker in the 9422 devices?
Issue:
On the 9422 mechanisms, can molded case switches be used instead of KAL/KHL breakers?
Product Line:
Operating Mechanisms and Disconnect Switches
Environment:
9422 Operating mechanisms
Resolution:
Yes. Molded case switch must be same frame size as required for the breaker type.
On the 9422 mechanisms, can molded case switches be used instead of KAL/KHL breakers?
Product Line:
Operating Mechanisms and Disconnect Switches
Environment:
9422 Operating mechanisms
Resolution:
Yes. Molded case switch must be same frame size as required for the breaker type.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: