Issue:
Part number for the Lug to Lug kit for separate mounting for NEMA Size 00B, 00C, 0 and 1
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
9065 Thermal Overload Relays
Resolution:
The 9999LL0 lug to lug kit will be required if straight pass through SSOLR windows is not desired. This kit includes (3) bus bars, (2) terminal shrouds, and (6) lugs suitable for #14 to #4 AWG copper wires. This kit is only suitable for use with the NEMA size 00(b), 00(c), 0 & 1 solid state overload relays..
Additional information can be found by accessing the attached Instruction Bulletin.
Part number for the Lug to Lug kit for separate mounting for NEMA Size 00B, 00C, 0 and 1
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
9065 Thermal Overload Relays
Resolution:
The 9999LL0 lug to lug kit will be required if straight pass through SSOLR windows is not desired. This kit includes (3) bus bars, (2) terminal shrouds, and (6) lugs suitable for #14 to #4 AWG copper wires. This kit is only suitable for use with the NEMA size 00(b), 00(c), 0 & 1 solid state overload relays..
Additional information can be found by accessing the attached Instruction Bulletin.