Issue:
Product design features
Product line:
Enclosed residential circuit breakers
Environment:
QOM2 Circuit breaker enclosures
Cause:
Application
Resolution:
The QOM2E2200NRB consists of a QOM2200VH circuit breaker, QOM22225NRB(NEMA 3R) enclosure, a solid neutral assembly and a PKOGTA2 equipment ground bar kit.
NOTE: The QOM2E2200NRB is ONLY sold through the retail channels.
Product design features
Product line:
Enclosed residential circuit breakers
Environment:
QOM2 Circuit breaker enclosures
Cause:
Application
Resolution:
The QOM2E2200NRB consists of a QOM2200VH circuit breaker, QOM22225NRB(NEMA 3R) enclosure, a solid neutral assembly and a PKOGTA2 equipment ground bar kit.
NOTE: The QOM2E2200NRB is ONLY sold through the retail channels.
Released for:Schneider Electric Canada